Other Parts Discussed in Thread: ADC12D1000RF,
Hi.
I am using a LM95233 temperature sensor in its default configuration to monitor temperature of ADC12D1000RF IC. However, i am getting a reading of 1 degree Centigrade continuously which doesn't look like the actual temperature of the IC being monitored. What adjustment do i need to make? Also please let me know the correct configuration of the diode select register in this case. Should i configure it for 65 nm or 90 nm process or an MMBT3904 transistor?