This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: If AWR1642 isolate Digital ground and Analog ground, any risk?

Part Number: AWR1642

Could we use the bead to isolate Digital ground and Analog ground of AWR1642 CPU?

We found the noise is from PMIC's PWM switch GND noise-~4MHz.

It may have less GND plane to impact CPU's temp, but CPU's temp GND should be Digital ground, right?

Best Regards,

  • Hello Charles,
    We do not recommend separating the digital and analog grounds, that would not be easy to do on such a complex SoC. On our EVMs we use a single solid ground plan and lot of GND vias to provide the lowest possible GND impedance .

    The 4Mhz switching frequency noise would be coming from the supply and not the ground. So you can improve the filtering on the RF and analog supply lines. Also the switcher should be well isolated from the sensitive circuitry of the AWR device like XTAL lines, 1V4_APLL, 1V4_SYNTH o/p pins etc..

    Regards,
    Vivek
  • HI Vivek

    We found that noise is from PWM swith GND, not power supply, because our board design don't have enough board space to let RF antenna keep away from  power componenets.

    PS: RF antenna is on top side of PCB, but another side(bot side) is for Power components .ex: PMIC, and "12V=>5V" PWM power solution.

    It just wants to isolate digital and analog ground, but I knew AWR1642 document don't have the suggestion.

    So do you have any concern or risk to let us check? Or how to do the design? Thanks,

  • Hello Charles,
    Could you provide details on how you concluded the coupling is from the GND and not supply? Do you have solid ground planes on your board?
    One care about to take is to keep all the power routing away from the XTAL lines of the AWR device, this node can easily pick up surrounding noise since its an high impedance node.

    Regards,
    Vivek
  • HI Vivek

    Our PCB is 8 layers design. L1/L2 are rogers RO3003 and L5~L8 layers are FR4. L2 is for whole antenna's reference GND of rogers RO3003 and L5/L7 are for whole GND. So total have solid GND planes on our boards, and I think GND plane is enough. But it is not good design for the placement overlap between top side-PCB antenna and  bot side- PMIC power design, so it seems antenna is coupled from PWM Switch GND noise.  

    Below analysis is why we think RF spur is from PWM switch GND , not from power supply.

    1.) enable PMIC(LP87524B/J-Q1) Spread-Spectrum Mode to reduce 4MHz Switching Frequency noise.

          it can reduce 10dBc.( orignal noise: noise floor: 45dBc/ this RF spur: 63dBc, then if enable SSM, it becomes 53dBc from 63dBc.)

    2.)When rework another one board provide power supply/GND -" PMIC*4 power-3.3&1.8&1.2&2.3V, GND" to  2nd DUT" , 2nd DUT don't have RF spur.

        PS: PMIC power of 2nd DUT don't work, so don't have 4Mhz switch frequency noise   

    3.) When rework another one board provide power supply/GND -" PMIC*2 power-1.2&1.8V" to 2nd DUT, 2nd DUT still don't have RF spur.

         But when only add 2.3V power loading(ps: add one parallel 5 ohm on 2.3V power supply), it becomes to have  this RF spur.

        PS: PMIC*4 power consumption checking is as below.

              When 2nd DUT remove 1.2V/1.8 power supply from another one board power supply, 2nd DUTdon't have RF spur. Then when 2nd DUT add 2.3V power loading(PS: parallel 5 ohm), it still has RF spur .        

              (1) 3.3V- lowest power current.

              (2) 1.2V-~ 800mA( peak)

              (3) 1.8V-~1.2~1.3A(peak)

              (4) 2.3V-~400mA(peak)

     

     

     

     

     

  • Hello Charles,
    Thanks for sharing the details. From the experiment it seems like its supply coupling.
    I assume you are using the LP87524B PMIC followed by LDOs to get 1V o/p from the 1.8V rail and 1.8V o/p from the 2.3V rail.
    I did not understand the power supply loading with 5 ohms, could you elaborate on that a little? On which board did you put the load, the DUT #1 from which you are deriving the 2.3V supply or on the DUT #2 board? So just putting additional load causes the spur to show up?

    Regards,
    Vivek
  • Hi Vivek

    Our design is co-layout LP87524B and LP87524J, and the analysis is the same result about PWM switch GND noise if follow up our check items.

    We add 5 ohm parallel on  2.3V's output. It means 2.3V add  2.3V/10 ohm power current.

    DUT1/DU2 two are for the same design boards. DUT1 is only for power supply and GND and DUT2 is for RF spur measurement board.

    As list to you about item2 last feedback, 

         (2) We rework to turn off DUT2's PMIC*4 power , and then use wire to connect DUT1's power supply , so DUT2 board don't have PMIC 4MHz PWM  switch frequency , and DUT2 use the same design power

              supply from DUT1. It seems RF spur disappear.

    As list to you about item3 last feedback, 

         (3) We also rework to trun off DUT2's PMIC's 1.2V&1.8V(ps: 3.3V&2.3V still work on DUT2), and then use wire to connect DUT1's PMIC's 1.2V&1.8V.

              So DUT2 board also have 4MHz PWM switch frequrency, but this noise should be lower. It seems RF spur disappear.

             next step, 

                            We only rework to add DUT2's 2.3V's power loading(PS:  add 5 ohm parallel on  2.3V's output. It means 2.3V add  2.3V/10 ohm power current.), so PWM 4MHz PWM  switch frequency becomes     

                            strong.

                            Then this measurement could get RF spur for 4Mhz noise.            

     

        So why do you still think it is power supply coupling, not for PMIC PWM swith GND?           

                   

  • Hello,
    It could be either supply or GND coupling from the PMIC to AWR device. To avoid this two need to properly isolate the PMIC from the critical sections of the AWr device, like the XTAL pins, 1V4 APLL, 1V4 SYNTH, BGAP. The GND return currents of the PMIC can be localized to PMIC and preventing them to cut through the AWR device currents by providing cuts on the GND layer between the PMIC and AWR device.

    Regards,
    vivek