Tool/software: Code Composer Studio
Device AWR1443
SDK 2.1.0.4
Custom upgraded toolbox 3.1.1 High accuracy lab such that it operated with SDK2.1.0.4 so that i could run this demo on silicon version ES 3.0
I can connect to tthe target in the high accuracy visualiser, but when i try to send it the configuration file i get the following error
"Error: Incorrect config reported by target. Hint: Change configuration and try again"
I'm unsure at this point whether this is an issue with my build or incompatibilitity between sdk2.1.0.4 and the visualizer.
What would produce this error on the visualiser side?
The visualiser as i understand only supports SDK 1.0.0 (in the about section of the visualiser)
Is there anyother way i can view this data?
Regards
Dan