Other Parts Discussed in Thread: MMWAVE-SDK,
Hi TI support team .
Have been trying the ROS demo visualizer lab.
Couple of observations and questions , hope you could clarify quickly.
1. Seems 'peakGrouping' is not supported in .cfg ( Seems support exists for 1642 and 1443) . An earlier discussion in the forum seems to suggest that with this command, we could define the
min and max range for detection , while disabling the peakGrouping option in "cfarcfg" for Doppler and range.
2. I used the "mmwave Demo visualizer" to create a .cfg . It doesn't allow opting in/out of peakGrouping of Doppler / range , and static clutter. peakGrouping is enabled and Static clutter is disabled.
3. mmWave estimator - chirp configurator , saves in .json format. Is there a script to convert this to CLI compatible .cfg format ?
4. If the "clutterRemoval" is manually enabled, the RoS visualizer doesn't have any pointcloud data . the visualizer is empty.
5. Is there a means to capture Range/ Doppler Heat maps from ROS ( though Lab demo and do a 3D real time heat maps with some filtering ?
thanks
...ravi