TMP112AIDRLR is connected to an I2C bus along with other I2C slaves. The design is same as Figure 17 of datasheet (SBOS473H–MARCH 2009–REVISED OCTOBER 2018). The filtering resistance is also added as per Figure 18. All the other slaves on I2C bus are functioning properly. But the SDA logical high voltage level is lower than expected when TMP112 is transmitting. The situation didn't change when a pull-up resistor of 1.6kohms is used on SDA. Voltage at V+ is 3.3V.