Other Parts Discussed in Thread: TMP107, TMP61
Hi,
We need air temperature sensor,by using sensors Monitor the Temperature of Refrigerator ,So I am Planing to use LMT86,The Temperature range to monitor -30C to 70C operating volatge is 3.3V,Sensor is mounting on one board and controller board is Placing down of the Refrigerator so we have to interface two boards with wire minimum 1 meter max 1.5 Meter, Sensor output type analog,Any extra circuit is neccesary for analog circuit like amplifier,Filter.
Suggest me LMT86 is suitable for my application or any alternate part number suggest quantity is 100k.