Other Parts Discussed in Thread: DRV5056, DRV5055
Dear all TI Engineers,
I need recommendation on MCU working with this sensor:
MCU must consume power which is low enough to be collected by energy harvester. ^^
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tim,
The DRV425 does consume max 10mA at 5V. Are you planing to cycle the power to the DRV425? This may be the only way you have low enough power for the DRV425 as it will already consume 50mW before you add the additional current required to drive the compensation coil. The amount of compensation current will be dependent on the magnetic field you are measuring. For example our transfer characteristic is 12.2mA/mT so if you were measuring 2mT there would be an additional current of 24.4mA.
Also are you planning to have the MCU do the measurements with an integrated ADC? What resolution are you attempting to get? The bandwidth will decrease with increase in Rshunt? How fast are you planning to get measurements and repeat it.
Tim,
There are two issues with using the DRV425. Its own power draw of the DRV425 by harvest power standards is large. The other is the DRV425 has a maximum range of approximately 2mT. We do have hall sensors to measure larger fields but the devices we currently have are designed to work with magnets and positioning so they are designed to drift the gain to match the magnet. The other difference is that hall sensors technology in general is they cannot measure as accurate but are less expensive. They also draw power and vary depending the version of the part. The DRV5055 is bidirectional and the DRV5056 is unidirectional but they draw similar current as the DRV425 but they do not increase current as the magnetic field increase.
Tim,
We have a few options and another will be available soon.
Please go to the product page of each device and click on tools and software to see all available options. I have added links below for convience.