Other Parts Discussed in Thread: IWR1642BOOST
HI ,
I want co connect iwr1642boost via arduino how can i send .cfg file & read the data (like you did in counting people lab via matlab)? even if i connect the arduino UART-USB to connect J8 (on IWR1642BOOST) so it does not recognize it (you dont have driver to arduino / arduino library that i can use).
other quistion : you have a driver that i can install so i could read the data from IWR1642BOOST (via XDS110 PORTS that do work for me in windows) to RaspbarryPI?
the goal is to be able to send cfg file and read the data from IWR1642BOOST (like you did in the counting people lab (lab 11) ' matlab) without Using windows computer (eg arduino or raspbarry pi ). my problen is that when im using Rasbbarry PI 2 Model B it dosent recognize the 2 "COM PORTS" XDS110 Class Application/User UART & XDS110 Class Auxiliary Data Port. (when Rasbbarry PI 2 Model B i will just overwrite your matlab code to python ) .
what can i do ????? im desperatly needs help.