I was just using the board and all of the sudden it shut off and now it won't power back on. I was told to take of D3 and see if it will power up but it still is not powering. When i connect a power supply the red 5V led (DS2) lights up for a very short moment before turning off. My immediate assumption is that something on the board is broken and is causing a short circuit. Is it possible that the LP87524BRNFRQ1 buck converter is broken and is causing a short circuit to protect the board from further damage?