This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP235: TMP235 Low temp reporting matters

Part Number: TMP235
Other Parts Discussed in Thread: UCD90124A

HI team:

our customer find an issue by using TI part TMP235A2DCKR output voltage abnormal at -40℃ again (Vout >1.5V ) ,the failure rate is 5/149=3.36%,the failure DateCode is 1816,

more than 200 systems had been performed power cycling and stress testing in room(25'C), high(65'C), low temperature(-40'C),
 200*5=1000pcs TMP235 components are verified and ~8pcs malfunction when power up in -40'C.
TMP235 is connected to TI UCD90124A, I will attached  the issue report for the analysis.

thanks!TMP235 -40'C Mulfunction Issue_0222.pptx