hello,
i would to use the HDC1080 in my board, but i have a doubt about the temperature. i have a requirement on the operating temperature of-40°-85°.
in the HDC1080 datasheet, the humidity sensor Ambient Operating Temperature is -20°-70°, while the Functional Operating Temperature is -20°-85°. more, in the figure 3, it seems that the humidity sensor works up to -40°-85°.
can you explain me if the HDC1080 works correctly in -40°-85°?
thanks for the support
Fabrizio Gualtieri