Other Parts Discussed in Thread: TIDEP-0091,
I've been trying to scour the forums to get a better understanding of the range resolution and accuracy of the TIDEP-0091 demo program out of the box. I am attempting to us the IWR1443 to measure fluid level in an range of tank sizes, starting with 55 gallon drums and increasing from there. In test with a 55 gallon drum, I'm getting strangely repetitive measurements from the TIDEP-0091 setup.
For example, with the barrel filled with water so that the surface sits 17 inches from the surface of the IWR1443Boost board, the demo device is outputting 0.488641m, 0.451053m, and 0.526229m. When I raise the fluid level by 1 inch, I receive the same measurements from the device. This repetitive nature in values is seen across the range of fluid levels, causing me to question if the range accuracy of the demo configuration is equal to the range resolution of 3.75cm.
Please correct me if I am wrong, but I understand the base range resolution is limited to the 3.75cm due to the 4GHz range of the chirp frequency. I have read through several related threads and have come to the understanding that the range accuracy is a function of the SNR, range resolution, and FFT size. Is a range accuracy of the base demo of 3.75cm to be expected without performing a zoom FFT?
Is there a demo project available yet that incorporates the zoom FFT into the low power fluid level sensor? The only zoom FFT project that I have found is based on the old SDK, so making the conversion is a bit over my head, and more time consuming that I can currently invest in this project.
For this particular project, an accuracy of 0.5 inches would be ideal. Any suggestions of how to achieve this would be much appreciated.
Thanks,
Chris