Part Number: TDC1000-TDC7200EVM
I am looking to start a project using TOF to detect liquid flow and am looking for the correct eval board. The TDC1000-TDC7200EVM, which I believe is the board that I want, is listed as Obsolete and End of Life on both DigiKey and Mouser. I have also come across TDC1000-GASEVM which is described as being optimized for gas sensors running at 500kHz but from my research I should be using 1000 kHz sensors. What eval board should I obtain for liquid flow detection?