Other Parts Discussed in Thread: HDC2010, HDC2080, ADS1118, MSP430G2553, ADS1013
Hi Sirs,
Sorry to bother you.
Need your assistance on temp. & humidity sensor survey; Combo sensor is good.
- temp sensor :
internal ambient temperature sensor sensing range of at least −30°C to +60°C with accuracy in the range ±0.3 °C in the operating
temperature range
- humidity sensor
Humidity accuracy within at least 2% RH between 20% and 60% (±3% from 0-20%, ±3% from 60-70%, ±4% 70-100%)
So does HDC1080 is a suitable solution? or have another solution can share?