While doing test with AWR1243BOOST EVM, there was an issue with captured data as below description.
* Symptom is that bit value suddenly changed (discontinuity) in the frame of captured ADC data
* When object is static, the data (sudden) change issue did not happen
* The issue happens sometimes (3~4 per 100 frames), when object is moving
* When issue happened, in the frame (one frame -> 512 ADC samples per chirp, 128 captured data), there was data change (discontinuity) at certain point
* Normal case, there is no (significant) bit data change in the frame
So, can you guess what kind of issue, and why the issue happens?
Thanks and regards,
Hayden