Other Parts Discussed in Thread: IWR1642
Hello there,
I am trying to capture raw ADC data from IWR1642BOOST (ES1) using MMWAVE_DEVPACK and TSW1400. I have walked through the tutorial and few posts in forum but still cannot get it working. Below is my software version and what I have learned from the posts:
- HSDC Pro 5.00. mmWave Studio 2.0.0.2 (I could not find radar studio, guess it's renamed to mmWave studio). mmwave_dfp_01_02_00_01.
- I made sure that no jumper on EVM (SOP1, 2 and 3 were NOT connected) and all 5 jumpers on the DEVPACK were connected.
- While I was usig ES1, DFP_00_06_00_05 was nowhere to be found, so I have tried the 07.04 and 1.00.02 bss and mss firmware.
- I have walked through the tutorial until SensorConfig.
I have the following questions:
- When I selected the firmware at the start of HSDC Pro, all I could select was AR12xx- or AR16xx. Are they compatible with the IWR1642?
- The Lane 3 and 4 couldn't be selected.
- I clicked the "SetUp TSW1400" and "TSW1400 ARM" and in the HSDC Pro window it showed it was TRIGGER ARMED with yellow background. However, after I clicked "Trigger Frame", nothing showed up in the HSDC Pro and therefore no ADC data has been captured or the hardware was never actually triggered.
Is there anything I did wrong in the process or wrong firmware/software I used? Thank you in advance for any help!