HI,
Could you explain the meaning of "snr" in the Point Could array. How does it calculated ?
In our test, the snr of points which target index "254" and " 255" were almost same value of the normal target's points.
They are considered as outside of boundary or as noise, so they supposed to be small value, aren't they ?
The tested package is following.
ti\mmwave_industrial_toolbox_3_3_1\labs\lab0020_pplcount_Overhead\GUI_A_base_no_logic
Best Regard,
Fountain