Part Number: IWR1443BOOST
Tool/software: Linux
Hi
I have a doubt about how to handle the data from the IWR1443Boost. I am using SDK 2.1 and ES 3.0.
I have managed to get the log magnitude range and range doppler heat map data coming from the IWR1443Boost by modifying the ti mmwave ros package and the config.cfg.
From what I have read on the doxygen of the sdk, I realized that the data comes as uint16_t, and that is how I have stored the data.
However, on the documentation it says also that the log magnitude range is in the Q9 format. Does that mean that I have to rearrange the data that comes in 16 bits to sequences of 10 bits each and then convert it from Qformat? I have uploaded a picture of my log magnitude range using the 16 bits without doing the conversion. Could you also inform me if that is a reasonable result ?
Best Regards,
Daniel