Other Parts Discussed in Thread: FDC2212, FDC1004
I'm evaluating if LDC1612 could be used to detect targets with 3mm diameter. The detection distance is 0-1mm with resolution requirement of around 0.01mm. The max coil size is around 3mm. The WeBench could not find suitable coil solutions for this. Should I look into capacitive measurements instead with FDC1002? The device is relatively well shielded but the inductive measurement would probably be more resistant to outside noise.