Hi Team,
The customer designed the 1243P board. He is now connected via the 60Pin interface on the DCA1000. There is no XDS100 module on the 1243P board. How can he use the mmWave Studio to collect 1243P ADC data through DCA1000?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
The customer designed the 1243P board. He is now connected via the 60Pin interface on the DCA1000. There is no XDS100 module on the 1243P board. How can he use the mmWave Studio to collect 1243P ADC data through DCA1000?
Thanks.
Hi,
XDS100 is being used for RS232 connection in SOP-2 mode to download the firmware.
If this interface is not available then the customer can work in SOP-4 mode and download the firmware over SPI (60 pin interface).
Regards,
Jitendra