This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: SPI connectivity lab

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: MMWAVE-SDK

Hi,

Is there any spi connectivity lab or example?

Thanks.

HONG.

  • Hi Hong,

    Please check the MMWAVE-SDK SPI driver test available in the following directory. It includes the source code and a pre-compiled binary that you can load from CCS. Additionally, it also includes a host side utility which you can run on a Windows 7 host to communicate with the SPI test binary running on the mmWave EVM.

    Device side test

    C:\ti\mmwave_sdk_02_01_00_04\packages\ti\drivers\spi\test

    SPI host utility

    C:\ti\mmwave_sdk_02_01_00_04\packages\ti\drivers\spi\test\windows

    Thanks

    -Nitin