Hi,
To evaluate people tracking/counting performance in our environment, I have changed the parameters in cfg file.
The reason of the change is there are restrictions in our environment as following,
- Bandwidth shall be smaller than 0.5GHz.
- Duty cycle shall be smaller than 7%
The test have done using following demo.
\ti\mmwave_industrial_toolbox_3_4_0\labs\lab0020_pplcount_Overhead\GUI_A_base_no_logic
Although I had prepared that range accuracy would be poor because bandwidth became narrow, I found some more issues.
- There are only few points associated to the person.
- There are many points associated to the ID 255.
Would you tell me which parameters should be change to achieve better performance ?
Please find attached the cfg file.
Best regards,
Fountain