Other Parts Discussed in Thread: ADS1235
Hello team,
Customer is looking for an integrated solution for strain gauge measurement. The main goal is to measure strain on a flex cable that is suspected of causing problems in assembly. Hence, the resistance may be in the very low (20 ohm range). I see for PGA302 in the previous post it's stated that with 2.5V excitation min resistance would be 300 Ohm.
Is there a way to use PGA302 for smaller resistance? Or maybe another part that we'd recommend instead of the PGA302?
I was looking at ADS1235 specs, not sure if that would work either. Appreciate your feedback.
Thanks!