Part Number: AWR1843
Other Parts Discussed in Thread: MMWAVE-SDK
Tool/software: TI-RTOS
Hi,
I am using AWR1843, on mmwave_sdk_03_02_00_04 in MCAN CANFD default demo test code is not seems to working, I am using PEAK CAN software to interpret CANFD messages and found data phase error while having the baud rate configured correctly(i.e Nominal and Data bit rate are 1Mbps and 8Mbps respectively).
In MCAN the classic CAN is working fine with Nominal bit rate of 1Mbps, able to receive and send messages.
Please clarify how to configure or make CANFD in working state.
PFA.
Thanks,
Vikas Patil