Hello support team,
Tx output power back-off of Tx2 and Tx3 does not work. It's work for Tx1 normally. Is something wrong with my config file?
Condition:
IWR1443BOOST ES3.0 with SDK2.1.0.4 demo binary image,
mmWave Demo Visualizer 2.1.0,
The target is a corner reflector made by bonding three 10 cm square metal plates with ~3.33m away from EVM.
Config files are attached.
Reading of Range Profile Zero Doppler (dB) of visualizer is:
Tx1 txOurPower 0, 10, 20, 30 = 115.8965, 105.3605, 94.82455, 85.79355.
Tx3 txOurPower 0, 10, 20, 30 = stuck to 117.4017
Tx2 txOurPower 0, 10, 20, 30 = stuck to 160.5493
Best Regards,
Katsuhiro