Tool/software: Code Composer Studio
Hi !
I'm currently working with LRPC Lab from Industrial Toolbox 3.6, with CCS 8.3.1 and SDK 3.1.1.2.
I'm using the ccs project of the Lab but with my own visualizer. When I send the first config after running the project in CCS, all is okay. But when I send a new config, to compare received datas with the previous one, an error occur in CCS and I have to remove my configuration and reset the board.
Where this issue can come from please ?
Here is my config : LRPC_demo_default.cfg
And this is my CCS Console :
[C674X_0] Debug: Logging UART Instance @00815f38 has been opened successfully Debug: DSS Mailbox Handle @0080c2f8 Debug: MMWDemoDSS create event handle succeeded Debug: MMWDemoDSS mmWave Control Initialization succeeded [Cortex_R4_0] ********************************************** Debug: Launching the Millimeter Wave Demo ********************************************** Debug: MMWDemoMSS Launched the Initialization Task Debug: System Heap (TCM): Size: 98304, Used = 4904, Free = 93400 bytes Debug: MMWDemoMSS mmWave Control Initialization was successful Debug: CLI is operational [C674X_0] Debug: MMWDemoDSS ADCBUF Instance(0) @00815f20 has been opened successfully Debug: MMWDemoDSS Data Path init succeeded Debug: MMWDemoDSS initTask exit [Cortex_R4_0] Error: MMWDemoMSS mmWave Stop failed [Error code -203227134] Debug: Heap before creating a tracker Debug: System Heap (TCM): Size: 98304, Used = 30016, Free = 68288 bytes Debug: (GtrackModuleInstance *)0x800a3e8 Debug: System Heap (TCM): Size: 98304, Used = 58768, Free = 39536 bytes Debug: MMWDemoMSS Received CLI sensorStart Event Debug: System Heap (TCM): Size: 98304, Used = 58768, Free = 39536 bytes Debug: MMWDemoMSS mmWave config succeeded [C674X_0] processCreate: (radarProcessInstance_t *)0x8007d8 processCreate: (RADARDEMO_rangeProc_handle *)0x8008a0 processCreate: (RADARDEMO_dopplerProc_handle *)0x800af8 processCreate: (RADARDEMO_detectionCFAR_handle *)0x801050 processCreate: (RADARDEMO_aoAEstBF_handle *)0x802434 processCreate: (RADARDEMO_clusteringDBscanInstance *)0x3a4bf443 processCreate: (RADARDEMO_clusterTracker_handle *)0xd44f3b90 processCreate: (radarProcessBenchmarkObj *)0x807718 processCreate: heatmap (float *)0x20080000 DDR Heap : size 786432 (0xc0000), used 604048 (0x93790) LL2 Heap : size 45056 (0xb000), used 29236 (0x7234) LL2 Scratch : size 9472 (0x2500), used 9216 (0x2400) LL1 Scratch : size 16384 (0x4000), used 16384 (0x4000) HSRAM Heap : size 8192 (0x2000), used 0 (0x0) [Cortex_R4_0] Error: Asynchronous Event SB Id 15 not handled [C674X_0] Debug: MMWDemoDSS Received STOP Event Debug: MMWDemoDSS Received STOP Event {module#8}: "../dss_main.c", line 184: error {id:0x10000, args:[0x814194, 0x814194]} xdc.runtime.Error.raise: terminating execution [Cortex_R4_0] Debug: Heap before creating a tracker Debug: System Heap (TCM): Size: 98304, Used = 58640, Free = 39664 bytes Debug: (GtrackModuleInstance *)0x800a368 Debug: System Heap (TCM): Size: 98304, Used = 58640, Free = 39664 bytes Debug: MMWDemoMSS Received CLI sensorStart Event Error: MMWDemoMSS mmWave Configuration failed [Error code -203227134]
Thanks a lot !
Quentin