Hi! I have a customer looking to use the TMP461 with a question on the VIL spec in the datasheet. Would you be able to help shed some light on below question from customer?
I have a question about the TMP461 data sheet. The Serial Interface low level input voltage. The spec says 0.45V max, but the I2C spec states this should be 0.8V max. Can you verify the data sheet is correct? We are using it in an application where the master has a 0.4V Voh max, so we would have only 0.05V of noise margin.
Thank you,
Meredith