This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMP91000EVM: LMP91000 cannot be connected to a computer after the Sensor AFE software is upgraded

Prodigy 80 points

Replies: 4

Views: 114

Part Number: LMP91000EVM

In the past year, I have used the Sensor AFE Software for SPIO-4 board and LMP91000EVM  on several Windows 7 and Windows 10 computers. I know there is a problem with the LMP91000EVM software in 64-bit operating systems, but the "Enable Unsigned Drivers" solution  has been very successful.
In the last use, the software prompted me to check for updates. I chose "Yes" and then the software could no longer connect to the SPIO-4 board . Device manager of the computer  shows "Device is not installed correctly" . Moreover, the driver cannot be reinstalled correctly, even on Windows XP.

  • Bob - 

    can you confirm that you are unable to uninstall the program, reboot and re-install? 

    It seems no one has updated this software since 2012 and in this GUI, the 'Check Update" in Help drop-down leads to defunct National web address 

    BR-

    Josh

  • Josh-
    I am also not sure if the failure was caused by sofeware upgrade. But now several computers can't connect to the board.
    I tried uninstalling and reinstalling, and the drivers could not installed properly. Is there any way to solve this problem?
    Thanks!

    Bob



     

    A Message from the TI E2E™ Community
    Texas Instruments

     

    Josh Wyatt replied to LMP91000EVM: LMP91000 cannot be connected to a computer after the Sensor AFE software is upgraded.

    Bob - 

    can you confirm that you are unable to uninstall the program, reboot and re-install? 

    It seems no one has updated this software since 2012 and in this GUI, the 'Check Update" in Help drop-down leads to defunct National web address 

     

    BR-

    Josh

     

    You received this notification because you subscribed to the forum.  To unsubscribe from only this thread, go here.

    Flag this post as spam/abuse.

    refid:46fc556f-2824-4335-bc90-66b66dfcbad7

  • In reply to Bob Wren:

    Bob - 

    I am still need some more time to get this answer - again, sorry for the delay

    BR-

    Josh

  • In reply to Josh Wyatt:

    Bob - 

    did you ever get this to work on your side? we have installed it on multiple computers here and not run into same issue and we are not aware of anyone updating it recently. 

    BR-

    Josh

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.