This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Range and accuracy limitations of High accuracy firmware

Part Number: IWR1443
Other Parts Discussed in Thread: IWR1642BOOST

High accuracy firmware achieves ~1 mm accuracy through interpolation. Interpolation is performed through 16384 point DFT.

As there are 16384 points in output DFT, it is possible to achieve 1 mm accuracy up to 16384 mm (16.384 m).

Is it possible to achieve 1 mm accuracy up to 40 m or beyond using IWR1443?