Other Parts Discussed in Thread: LDCCOILEVM, LDC1612EVM,
Hello
I have the following questions. I was always wondering.
The coil design uses Spiral Inductor Designer, but there are things you want to check here.
For example, if the thickness of the two-layer coil and PCB is 1.5 mm, how should the distance between the coils in Spiral Inductor Designer be set? *
Should I set the “PCB thickness between 1st layer and 2nd layer” to 1.5 mm?
Looking at the Layer Stackup diagram, it seems that “PCB thickness between 1st layer and 8nd layer” is set for a 2-layer coil. But there is no place to set it. What should I do now?
What should I do for the 4-layer coil? *
Is there a description about the LDC1612EVM or LDCCOILEVM 4-layer PCB structure (thickness between layers) somewhere? If you don't know these, you won't be able to make the correct settings for Spiral Inductor designer PCB Thickness
Best regards