This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1080: Correct Device Behavior?

Part Number: HDC1080

I'm trying to understand whether I'm implementing this correctly in Verilog. Should I be expecting a STOP after the ACK when I transmit the trigger message. I get a STOP but maybe I shouldn't because it's not shown on the datasheet Figure 12. I'm configured for temperature and humidity in sequence. In addition, when I transmit a read message to obtain the measurements, I seem to get the first byte and it appears to be real. The first byte is ACK'ed. However, the remaining 3 bytes come back as 0xFF followed by NACKs. (the last byte should get a NACK - so that's ok).

Any ideas? Carmine Iascone, are you out there?