Hi
I'm using code composer 9.1.1.00010
unzipped 'TDC720xEVM_Firmware_Source-v2.07"
Imported into CC
And when I build i get the following errors
Can someone point in the correction direction to correct these.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm using code composer 9.1.1.00010
unzipped 'TDC720xEVM_Firmware_Source-v2.07"
Imported into CC
And when I build i get the following errors
Can someone point in the correction direction to correct these.
Thanks
David,
Please comment out the CSTRING in the code and then build this program, it should then compile without any errors.
The CSTRING is not needed for this program operation.