Other Parts Discussed in Thread: , LDCCOILEVM
I designed a coil Sensor using Coil designer Webench tool. 14mm OD, 24 turns, 2 layer, 4mils Trace width & 4 mils trace spacing, Cap is 330pF. I evaluate this Coil Sensor with the help of LDC1612EVM kit to detect the IDrive required as I don't know the Rp of the sensor. Am Using LPCMCU (I2C) to communicate with the LDC1612 IC. Do I require separate logic to write in the MCU to alter the optimal Oscillation Voltage given to the coil sensor? Because even after changing the drive current, the Vosc remains same while connected with MCU, but it changes while it is connected with EVM.
Kindly suggest the method/parameters to uniformly manufacture the Coil sensor PCB to use it in my application, or please share the gerber file for the same (Found in LDC Reference Coil User Guide - Sensor coil "M"). As of now I need to check and set the drive current for each and every coil sensors to use in the module.
Expecting your valuable inputs.
Regards,
Dinesh