This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Object data over CAN demo for AWR1843BOOSTER

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1642, AWR1843,

Hi,

i was going through object data over CAN demo.

i have found pre-build libraries for AWR1642.i'm wondering whether we shall flash this for AWR1843.

if there is any demo specific for AWR1843BOOSTER to get object data over can,Please share it.

Regards,

Vimal

  • Hi Vimal,

    You can build the same application for AWR1843 using CCS project, change the device type to AWR1843 in the CCS project properties(general option). And then flash the built binary file to AWR1843BOOST.

    That's the only reference application we have for mmwave sensor to send object data over CAN/CAN-FD. And that is almost same as mmw demo but the difference that instead of UART it uses CAN and all the configurations are embedded in the application source instead of taking over CLI UART from PC.

    Regards,

    Jitendra