Part Number: AWR1243BOOST
Dear ,
I am using AWR1243boost with Mmwave studio to processing RAW IQ data in matlab and configured the radar with 1 Tx and 4 Rx . For the testing purpose i enable the test source to emulate the target at different positions , Velocities and signal strengths.
I understood from the below link and documents that objects will be resolved in angle FFT.
https://e2e.ti.com/support/sensors/f/1023/t/768283?AWR1642BOOST-Angle-resolution-object-separation-at-80-m-range-to-show-them-as-different-trackers
I agree with the point mention below and verified by the test case mentioned below
A common case where the above assumptions fail is if the targets and the radar are both stationary. In such a case, if there are two objects at the same range (from the radar), they will remain at the same at that range indefinitely, and as such cannot be distinguished by the radar.
But please explain me why that cannot be distinguished by the radar because I have a targets as mentioned below where (RadarStudio PostProcessing matlab gui)we not able to distinguish both in angle
target 1 x = 0 , y= 40 , vx=0 ,vy =0.9
target 2 x = 25.70 , y= 30.64 , vx=0.7 ,vy =0.7
Please explain what is happening because i am pointless and new to this post processing.
To distinguish above targets and (static) target at the same range (from the radar), they will remain at the same at that range indefinitely what kind of technique need to be adapted .
Please help me in clarifying the doubt and reply as soon as possible.