We configured the AWR1443 to operate with 400 kHz I2C frequency, but it operates with 430 kHz.
The root cause seems to be I2CMasterInitClk, which uses a "d" of 6, independent of the prescaler. The reference manual (25.1.3 Clock Generation) says, "d" should be 5 for a prescaler > 1. Is there / will there be a fix in future MMwave SDK versions? We are using SDK 3.01.00.02