Other Parts Discussed in Thread: AWR1642
I have an issue with the sampling rate of the radar system even though I am just using the default settings for it in the Sensor Config tab.
This is using a DCA1000 with an AWR1643BOOST.
[14:51:38] RSTD.Build()
[14:51:38] RSTD.SaveSettings(): Settings saved to "C:\Users\weilu\AppData\Roaming\RSTD\config.xml"
[14:51:38] RSTD.Transmit("/")
[14:51:38] RSTD.AL_Build()
[14:51:38] RSTD.AL_LoadXml()
[14:51:38] RSTD.Transmit("/")
[14:51:38] RSTD.AL_Init()
[14:51:38] RSTD.Clients_Build()
[14:51:38] GM: Init
[14:51:38] GM: Loaded 'C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Clients\\LabClient.dll'
[14:51:38] GM: 1 Guest (s) init
[14:51:38] GM: 1 Module(s) init
[14:51:38] GM: 2 Tab (s) init
[14:51:38] RSTD.Client_LoadXml()
[14:51:38] [RadarAPI]: ar1.selectRadarMode(0)
[14:51:38] [RadarAPI]: Status: Passed
[14:51:38] Matlab Runtime Engine is installed
[14:51:38] [RadarAPI]: Starting Matlab Engine..
[14:51:42] [RadarAPI]: Matlab Engine Started!
[14:51:43] [RadarAPI]: ar1.selectCascadeMode(0)
[14:51:43] [RadarAPI]: Status: Passed
[14:51:43] [RadarAPI]: ar1.LoadSettings('C:\Users\weilu\AppData\Roaming\RSTD\ar1gui.ini')
[14:51:44] TESTING = false
[14:51:44] RstdNet: Port 2777: Listening..
[14:54:14] [RadarAPI]: Opening Gpio Control Port()
[14:54:14] [RadarAPI]: Status: Passed
[14:54:15] [RadarAPI]: Opening Board Control Port()
[14:54:15] [RadarAPI]: Status: Passed
[14:54:16] [RadarAPI]: ar1.FullReset()
[14:54:16] [RadarAPI]: Status: Passed
[14:54:16] [RadarAPI]: Closing Board Control Port()
[14:54:16] [RadarAPI]: Status: Passed
[14:54:16] [RadarAPI]: Closing Gpio Control Port()
[14:54:16] [RadarAPI]: Status: Passed
[14:54:16] [RadarAPI]: ar1.SOPControl(2)
[14:54:16] [RadarAPI]: Status: Passed
[14:54:18] [RadarAPI]: ar1.Connect(9,921600,1000)
[14:54:20] [RadarAPI]: Warning: Connected with baudrate 115200
[14:54:21] [RadarAPI]: Warning: Disconnected existing BaudRate
[14:54:21] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[14:54:23] [RadarAPI]: ar1.Calling_IsConnected()
[14:54:24] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[14:54:24] [RadarAPI]: Status: Passed
[14:54:24] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[14:54:24] [RadarAPI]: Status: Passed
[14:54:24] [RadarAPI]: ar1.deviceVariantSelection("XWR1642")
[14:54:24] [RadarAPI]: Status: Passed
[14:54:24] [RadarAPI]: ar1.frequencyBandSelection("77G")
[14:54:24] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[14:54:24] [RadarAPI]: Status: Passed
[14:54:24] Device Status : XWR1642/ASIL-B/SOP:2/ES:2
[14:54:24] [RadarAPI]: ar1.SaveSettings('C:\Users\weilu\AppData\Roaming\RSTD\ar1gui.ini')
[14:54:26] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss\\xwr16xx_radarss.bin")
[14:54:26] [RadarAPI]: Downloading BSS Patch RPRC Binary..
[14:54:28] [RadarAPI]: ar1.GetBSSFwVersion()
[14:54:28] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[14:54:29] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[14:54:29] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
[14:54:29] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\masterss\\xwr16xx_masterss.bin")
[14:54:30] [RadarAPI]: Downloading MSS RPRC Binary..
[14:54:31] [RadarAPI]: ar1.GetMSSFwVersion()
[14:54:31] [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
[14:54:33] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[14:54:33] [RadarAPI]: Status: Passed
[14:54:33] MSS power up done async event received!
[14:54:35] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[14:54:35] [RadarAPI]: Status: Passed
[14:54:35] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[14:54:35] [RadarAPI]: Status: Passed
[14:54:35] Device Status : XWR1642/ASIL-B/SOP:2/ES:2
[14:54:35] [RadarAPI]: ar1.RfEnable()
[14:54:35] [RadarAPI]: Status: Passed
[14:54:35] BSS power up done async event received!
[14:54:35] [RadarAPI]: ar1.GetMSSFwVersion()
[14:54:35] [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
[14:54:36] [RadarAPI]: ar1.GetBSSFwVersion()
[14:54:36] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[14:54:37] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[14:54:37] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
[14:54:38] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[14:54:39] [RadarAPI]: Status: Passed
[14:54:41] [RadarAPI]: ar1.LPModConfig(0, 1)
[14:54:41] [RadarAPI]: Status: Passed
[14:54:41] [RadarAPI]: ar1.RfInit()
[14:54:41] [RadarAPI]: Status: Passed
[14:54:41] RF Init async event received!
[14:54:41] [RadarAPI]: Time stamp, Temperture: 6535,44; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 0, 0; RxIQMM Status, Update: 1, 1;
[14:54:55] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
[14:54:55] [RadarAPI]: Status: Passed
[14:54:57] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[14:54:57] [RadarAPI]: Status: Passed
[14:54:58] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
[14:54:58] [RadarAPI]: Status: Passed
[14:55:07] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[14:55:07] Status: Failed, Error Type: SAMPLING RATE IS NOT WITHIN [2, 37.5] Msps