Other Parts Discussed in Thread: DRV5057, DRV5055, DRV5053, DRV425
Hi team,
Do we have similar part compete with HW-101A-FG as attachment?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello James,
The HW-101A is a raw Hall element, and TI only has Hall ICs. From the function of the HW-101A, I believe a linear magnetic sensor would best suite your needs.
For Hall effect sensors, we have the DRV5053, DRV5055, DRV5056, and DRV5057. Of these, the DRV5056 is the closest to the same function, but does not have the same type of sensitivity.
Because of the high sensitivity of the HW-101A, I would recommend looking into the DRV425. This is a highly sensitive linear magnetic sensor (fluxgate technology) with adjustable gain and range.