I am working to hard code a chirp configuration into the vehicle occupancy + vital signs demo included in the Automotive Toolbox version 2.7.1.
I have modified cli.c to iterate through an array of strings which contain the commands I need. Some chirp commands are accepted while others are not recognized by the system. The commands which are not recognized are listed below.
I don't think I am starting the mmWaveExtensionHandler properly. I see other code using it to handle certain commands. I suspect the commands which fail are handled by the BSS processor and must be passed through mmWave Extension.
Failed Commands:
flushCfg
dfeDataOutputMode 1
adcCfg 2 1
adcbufCfg -1 0 0 1 1
profileCfg 0 77 250 10 40 0 0 90 1 64 2200 0 0 40
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 168 0 107 1 0
lowPower 0 1