Hi,
I set the "Antenna Config (Azimuth Res - deg)" to "4Rx,2Tx(15 deg)" in the mmWave Demo Visualizer.
I got a detection at (x, y) = (-2.978515625, 6.697265625) and the corresponding azimuth is atan(x/y) = -23.9764405 degree,
this azimuth value is not a multiple of 15 degree.
Does the "azimuth resolution = 15 degree" setting suggest that I could only get a measurement with multiple of 15 degree such as 0 degree, +/- 15 degree, +/- 30 degree, etc.?
Thanks for your help
Edward Lee