Other Parts Discussed in Thread: UNIFLASH,
Hi there,
i am unable to connect my IWR6843ISK to the demo visualizer. I am able to run the IWR6843ISK traffic monitoring labs and i am able to use uniflash to flash the metadata into the IWR6843ISK to do the traffic monitoring demo using the GUI application. During the setup of the IWR6843ISK i have correctly using the correct serial port. But whenever i press "send config to the mmwave device" it will show that com port 10 is "waiting for data". I am hoping if someone could provide me some directions on how should i go about troubleshooting. I have tried many stuff and so far i can't seem to breakthrough this problem.
Some questions i have back in my mind are:
May i know when using the demo visualizer, do i need to short my SOP2 pin in "flashing" or "operational" mode?
Do i need to flash any configuration file into the device using uniflash?