Other Parts Discussed in Thread: AWR1443, SN65HVDA540
Hello,
As i am having AWR1443 Boost with with PROC010 REV A . As per the AWR1443 user guide which says
2.4.3 CAN Interface Connector (for AWR1443)
The J3 connector provides the CAN_L and CAN_H signals (see Figure 8) from the onboard CAN
transceiver (SN65HVDA540). These signals can be directly wired to the CAN bus.
Because the digital CAN signals (TX and RX) are muxed with the SPI signals on the AWR device, one of
the two paths must be selected. To enable the CAN interface, the R11 and R12 resisters muct be
populated with 0 Ω, and the R4, R6, R28, and R63 resisters must be removed to disconnect the SPI path.
i made those changes,even then also i am not able see any data over CAN. I using mmWaveDemo Visualizer to run the EVM. I am able to see plots but cant see any data over CAN.
In order to observer the data over CAN what n all steps do need to follow ,please advice on that.