Part Number: IWR6843ISK-ODS
Hi,
I want to configure the ES 2.0 ODS board to have the full +/- 60 degrees FoV for both azimuth and elevation. I rebuilt the new 3D people counting lab DSS and MSS using "method 2" to have the larger, pre-defined L2/L3 cache for full FoV support. However, I was only able to configure the ODS to be +/- 50 degrees in both azimuth and elevation. The demo would not pass calibration stage if I feed any larger value to config.
Could you provide some guidance for getting the full FoV running for this lab?
Thanks in advance,
Bing