Is there a way to test the config serial port and the data serial port without using the usb on the IWR1443 evaluation board. I only see one Rx, Tx pair (pin5, pin6) available on the J6 connector. Using the mmWave Demo Visualizer I have to send configuration commands and receive data on two separate serial ports...