Hi team,
Looking at Figure 14, it says "Delay is set by CR1 and CR0". I believe "Delay" means "conversion time".
According to electrical characteristics, conversion time is fixed value.
1. Is there any relation with conversion rate and conversion time?
2. Could you make sure whether conversion time is changed by CR1 and CR0 or not?
Also, I want to make sure the reliability of first data just after powering up.
The subsequent data after first data needs 250ms(default), but the first data only waits 25ms.
So, I'm concerned about the reliability of the first data.
3. Could you confirm if the reliability or accuracy is the same between first data and subsequent data?
4. Is there any power up condition that degrades the reliability of first data?
5. To make sure the first data reliability, could you check how much time the internal oscillator needs to be stable after powering up?
Regards,
Saito