This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: DSP/DSS control and debug from the MSS

Part Number: AWR1843


The following questions pertaint to reset and debug control of the DSS from the MSS side.

The application  is running from internal SRAM and any reset or SOFTRESETREQ will rerun the bootloader

and overwrite the information he has downloaded to RAM with the contents from ext. flash.

We have addressed this by enabling ROM eclipsing and performing CR4 reset using the MSS_RCM:SOFTRST1 register.

The question here is if the VIM should be soft reset as well using the SOFTRST2 register?

 

The second question is on how to restart or control the DSP after a download to the DSP memories. The TRM under

27.2 mentions a Coresight cross trigger module CT-CTA to which the C674x megamodule is connected and which

according to the manual (see figure 27-3):

 

The second CTI module is present inside the debug subsystem. This CTI receives triggers from ADTF,

DMA, RTI, and WDT. GEM. The C674x DSP can be halted by any trigger in the subsystem. When GEM

trace is enabled, triggers are generated by ADTF by detecting the trigger packets in the trace stream.

 

However the manual does not state any specifics on this module and as it appears to be custom we would

need additional information on this module like component address, register map, functional description

etc. for CT-CTA component.

Can you elaborate on the CT_CTA component and the functionality of it?

What can the two triggers shown in the TRM do on the DSS side?

 

Alternatively is there a different way to soft reset the DSP from the CR4 side without rerunnig the bootloader?

Thank's in advance and Best Regards

Wolfgang Hoeld

  • Hi Wolfgang,

    Do you need to reset MSS/DSS under debug condition? If yes, then CCS IDE does that for you, where even after image loaded to DSS/MSS you can reset the cores and re-load the image and run. Or if you are trying to setup with different IDE?

    It would be good if you provide the usecase of reset/halt of the cores to help us understand more and provide the solution.

    Regards,

    Jitendra

  • Hello Jitendra,

    thank's for your reply. Iam aware that CSS does all this but we are a tools provider (iSYSTEM) and we need to

    implement a solution which is similar to what you do in CSS. However as outlined the key is to do all this from

    the CR4 side without touching the DSP Megamodule debug throug the IcePick. Hence, just the Coresight components

    is what we see from our debugger and we would need the sequence/access to properly reset and control the DSS

    side from that.

    Best Regards,

    Wolfgang Hoeld

  • Hi Wolfgang,

    I would suggest you refer C:\ti\<ccs path>\ccs_base\emulation\gel\xwr16xx_dss_init.gel file where it has functions to halt, reset of DSS core. All the addressing is from MSS core so you can use those addresses writing from MSS.

    To Reset DSS: WR_MEM_32(0xFFFFE10C, 0x070000AD); /* ASSERT RESET */

    WR_MEM_32(0xFFFFE10C, 0x07000000); /*De-ASSERT RESET */

    After this you can download image from MSS or from DAP then un-halt the DSS using above said gel file (Function DSS_ReleaseDSPHalt).

    You don't need to reset VIM after eclipsing MSS, as the application's driver initialization should do this reset usually.

    Regards,

    Jitendra

  • Hello Jitendra,

    thank you very much for your answers. I spent some time reviewing this agains the manual and have reviewed the

    gel files.

    The information on how to reset the DSS (soft reset) form the MSS is very clear and helpful (even the manual just

    lists that field/value 0xAD as reserved in the DSSCTL register at FFFFE10C.

    As far as halting/unhalting the DSS is concerned I found the functions in the xwr16xx_dss_cdap.gel file.

    I think this answers all the questions.

    Thank's and best Regards

    Wolfgang Hoeld

  • Hello Jitendra,

    after reviewing the .gel file I noted that there is one register which is used to check the power status of

    the DSS which I was not able to resolve - PWRAP_DPREC0 and it's associated bits. It looks like it

    might be a custom coresight component or access port?

    Could you elaborate on it pls.

    Best Regards,

    Wolfgang

  • Hi Wolfgang,

    Looks like it is DAP access port related variable used in the gel file. This is some variable used internally by CCS DAP which I don't find the explanation in the CCS

    Let me check with the concern team and get back to you.

    Regards,

    Jitendra

  • Hi Wolfgang,

    xwr16xx_dss_csdap.gel uses PWRAP_DPREC0 variable to check the DSS power-off or reset status. This can be checked using DSS_REG_GEMPWRSMCFG3_REG register.

     

    gempwrsmcfg3_rd = HW_RD_REG32(DSS_REG_GEMPWRSMCFG3_REG);

    power_status = (gempwrsmcfg3_rd >> 18) & 0x3 ;

    if((0x00000000 == (pwrap_dprec0_rd & 0x00000020)) || (0x00020000 == (pwrap_dprec0_rd & 0x0007C000)))     -->> if(power_status != 0x3)

    /* power_status == 3 means DSS is powered ON */

    Regards,

    Jitendra

  • hi Jitendra,

    o.k - I am checking the power status instead no problem. However the underlying problem is that I

    Halt the DSP the following way:

    1. Check PWRSTATUS - if ON proceed
    2. Info - GEMRSTCAUSE 0x00010101
    3. Set GEMPWRSMCFG4.PWRSMLRSTHALT
    4. Write 0x070000AD to 0xFFFFE10C
    5. Write 0x07000000 to 0xFFFFE10C
    6. Check PWR status = OFF
    7. Info - GEMRSTCAUSE 0x000B0B03

    To restart the DSP I implemented the steps in the xwr16xx_dss_csdap.gel file. However the problem is

    that despite of clearing GEMPWRSMCFG4.PWRSMLRSTHALT and unmasking GEMPWRSMCFG4.GEMEVENTMASK

    the PowerStatus remains 0x0 = OFF. Hence it seems I can properly stop the DSP with a local reset but I can not

    restart it.

    Any ideas on what to check or what could be wrong? Maybe the TI tools stop the DSP in a different way then I do?

    Thank's in advance for your help.

    Wolfgang

  • Hi Wolfgang,

    After reset (above sequence) you need to un-halt the DSS again (execute DSS_ReleaseDSPHalt function from *.gel file).

    Regards,

    Jitendra

  • Hello Jitendra,

    yes this is exactly what I am doing - as I wrote:

    To restart the DSP I implemented the steps in the xwr16xx_dss_csdap.gel file. However the problem is

    that despite of clearing GEMPWRSMCFG4.PWRSMLRSTHALT and unmasking GEMPWRSMCFG4.GEMEVENTMASK

    the PowerStatus remains 0x0 = OFF. Hence it seems I can properly stop the DSP with a local reset but I can not

    restart it.

     


    What I see is that device does not restart. The gel file has a section where it checks if the STC was triggered by

    the bootloader:

     // Check if DSS_STC is triggered by Bootloader
           if(0x1 == (stcgstat_rd & 0x1))
           {
               unsigned int stcpbistsmcfg1_rd = HW_RD_REG32(DSS_REG_STCPBISTSMCFG1_REG);
               unsigned int stcpbistsmcfg1_wr = 0;
               
               // Clear bit 3
               stcpbistsmcfg1_wr = stcpbistsmcfg1_rd & (~(1 << 3));  
               HW_WR_REG32(DSS_REG_STCPBISTSMCFG1_REG, stcpbistsmcfg1_wr);
           }

    That code was implemented as well and I see it being executed. Following it I unhalt the DSP power

    state machine by clearing GEMPWRSMCFG4.PWRSMLRSTHALT. I then poll the power status for 1 sec

    but it remains 00. Rerunning the function later stiil yields a power status of 00.


    I hope that makes clear what the problem is - it is restarting the DSP  with the sequence used in the

    gel function DSS_ReleaseDSPHalt().

    Has anybody successfully used this after halting the DSP with a reset?

    Best Regards

    Wolfgang

  • Hi Wolfgang,

    This is what I have tried at my end with AWR1843 device.

    1. Flash the mmw demo and run in SOP-4 mode. 

    2. Connect CCS to the device, able to connect MSS and DSS core.

    3. Disconnect DSS core but connect only MSS core.

    4. From MSS core: Write 0xFFFFE10C[0:7] = 0x070000AD and then 0x07000000 to reset the DSS. 

    - not able to connect to DSS core at this point 

    5. Then execute DSS_ReleaseDSPHalt function from the gel file.

    6. Now able to connect back to DSS core.

    So effectively with these steps, I'm able to reset the DSS core.

    Regards,

    Jitendra

  • Hello Jitendra,

    unfortunately this only prooves that the TI tools are working as expected. I believe the anser is in

    what is being done when the TI tools first connect to either core.

    I can see that the reset of the DSP core work as after that sequence the DSS is not powered/clocked and

    access to the DSP L2 and L1 memories is no longer possible.

    The problem is still with restarting the DSS side. Here is a log output of my script:

    I 01B : AWR1843 Release DSP from Halt after reset - STARTED
    I 01B :
    I 01B : Read:  0x500006C8
    I 01B : Value: 0x00014514
    I 01B :   
    I 01B :     DSP domain power status - GEM OFF
    I 01B : PWSMMODESTATUS 0x00000000
    I 01B :
    I 01B : Read:  0x500006CC
    I 01B : Value: 0x00FE0080
    I 01B :   
    I 01B :     DSP halted by PWRSMLRSTHALT - ok
    I 01B :
    I 01B : Read:  0x50040014
    I 01B : Value: 0x00000500
    I 01B :   
    I 01B :     DSS_STC was triggered by bootloader
    I 01B :
    I 01B : Read:  0x5000074C
    I 01B : Value: 0x00000018
    I 01B :
    I 01B : Write: 0x5000074C
    I 01B : Value: 0x00000010
    I 01B :   
    I 01B :     Clear GEMPWRSMCFG4.PWRSMLRSTHALT to restart the DSP
    I 01B :
    I 01B : Read:  0x500006CC
    I 01B : Value: 0x00FE0080
    I 01B :
    I 01B : Write: 0x500006CC
    I 01B : Value: 0x00FC0080
    I 01B :   
    I 01B :     Unmask/clear GEMPWRSMCFG4.GEMEVENTMASK
    I 01B :
    I 01B : Read:  0x500006CC
    I 01B : Value: 0x00FC0080
    I 01B :
    I 01B : Write: 0x500006CC
    I 01B : Value: 0x00F80080
    I 01B :   
    I 01B :     Waiting for DSP to power up
    I 01B :
    I 01B : Read:  0x500006C8
    I 01B : Value: 0x00014514
    I 01B : PWSMMODESTATUS 0x00000000

    This goes on until a timeout (1 sec) ...... occurs

    I 01B : Read:  0x500006C8
    I 01B : Value: 0x00014514
    I 01B : PWSMMODESTATUS 0x00000000
    I 01B :   
    I 01B :    DSP did not power up - TIMEOUT!
    E 01B : Power up of DSP timed out

    If I understand the manual correctly the DSP side requires a trigger in order to wake up. I get this from

    the RM 4.4.2.2 Power ON Control Sequence under items #2 and #4 it states to unmask the wakeup

    event and to trigger a wakeup event. Hence the gel file sequence is only a subset of this whole procedure

    described in the refmanual.

    In addition there are two additional access ports and from waht I  analyzed one is most likely the one

    holding the Power_DPRegs(s) registes while the other could be the one associated with the triggers from the MSS

    coresight modules to the DSS side:

    AP:sel:0x0000000004000000, id:0x002e0001  (AP is NOT ARM)
    AP:sel:0x0000000005000000, id:0x34770002  (ARM APB2-AP)
    AP:sel:0x0000000006000000, id:0x54770001  (ARM AHB3-AP)
    AP:sel:0x0000000007000000, id:0x002e0002  (AP is NOT ARM)


    Could you pls elaborate on the above points:

    1. Trigger required to restart the DSS and how to generate them?
    2. Additional access ports and their functionality (trigger? Power_DPRegs

    Thank's and Best Regards,

    Wolfgang

  • Hello Jitendra,

    unfortunately this only prooves that the TI tools are working as expected. I believe the anser is in

    what is being done when the TI tools first connect to either core.

    I can see that the reset of the DSP core work as after that sequence the DSS is not powered/clocked and

    access to the DSP L2 and L1 memories is no longer possible.

    The problem is still with restarting the DSS side. Here is a log output of my script:

    I 01B : AWR1843 Release DSP from Halt after reset - STARTED
    I 01B :
    I 01B : Read:  0x500006C8
    I 01B : Value: 0x00014514
    I 01B :   
    I 01B :     DSP domain power status - GEM OFF
    I 01B : PWSMMODESTATUS 0x00000000
    I 01B :
    I 01B : Read:  0x500006CC
    I 01B : Value: 0x00FE0080
    I 01B :   
    I 01B :     DSP halted by PWRSMLRSTHALT - ok
    I 01B :
    I 01B : Read:  0x50040014
    I 01B : Value: 0x00000500
    I 01B :   
    I 01B :     DSS_STC was triggered by bootloader
    I 01B :
    I 01B : Read:  0x5000074C
    I 01B : Value: 0x00000018
    I 01B :
    I 01B : Write: 0x5000074C
    I 01B : Value: 0x00000010
    I 01B :   
    I 01B :     Clear GEMPWRSMCFG4.PWRSMLRSTHALT to restart the DSP
    I 01B :
    I 01B : Read:  0x500006CC
    I 01B : Value: 0x00FE0080
    I 01B :
    I 01B : Write: 0x500006CC
    I 01B : Value: 0x00FC0080
    I 01B :   
    I 01B :     Unmask/clear GEMPWRSMCFG4.GEMEVENTMASK
    I 01B :
    I 01B : Read:  0x500006CC
    I 01B : Value: 0x00FC0080
    I 01B :
    I 01B : Write: 0x500006CC
    I 01B : Value: 0x00F80080
    I 01B :   
    I 01B :     Waiting for DSP to power up
    I 01B :
    I 01B : Read:  0x500006C8
    I 01B : Value: 0x00014514
    I 01B : PWSMMODESTATUS 0x00000000

    This goes on until a timeout (1 sec) ...... occurs

    I 01B : Read:  0x500006C8
    I 01B : Value: 0x00014514
    I 01B : PWSMMODESTATUS 0x00000000
    I 01B :   
    I 01B :    DSP did not power up - TIMEOUT!
    E 01B : Power up of DSP timed out

    If I understand the manual correctly the DSP side requires a trigger in order to wake up. I get this from

    the RM 4.4.2.2 Power ON Control Sequence under items #2 and #4 it states to unmask the wakeup

    event and to trigger a wakeup event. Hence the gel file sequence is only a subset of this whole procedure

    described in the refmanual.

    In addition there are two additional access ports and from waht I  analyzed one is most likely the one

    holding the Power_DPRegs(s) registes while the other could be the one associated with the triggers from the MSS

    coresight modules to the DSS side:

    AP:sel:0x0000000004000000, id:0x002e0001  (AP is NOT ARM)
    AP:sel:0x0000000005000000, id:0x34770002  (ARM APB2-AP)
    AP:sel:0x0000000006000000, id:0x54770001  (ARM AHB3-AP)
    AP:sel:0x0000000007000000, id:0x002e0002  (AP is NOT ARM)


    Could you pls elaborate on the above points:

    1. Trigger required to restart the DSS and how to generate them?
    2. Additional access ports and their functionality (trigger? Power_DPRegs

    Thank's and Best Regards,

    Wolfgang

  • Hi Wolfgang,

    We are checking this with the team internally. We will update you soon.Thanks for your patience.

    Meanwhile, Instead of resetting DSP, you can reset the PC to first location so application can start executing from the beginning again.

    Regards,

    Jitendra

  • Hello Wolfgang,

    Based on internal team response: 

    He needs to follow the exact power on sequence as mentioned in the TRM :

     

    3.4.2.2 Power ON Control Sequence

    Below is the detailed sequence to power on the DSP.

    Master subsystem-controlled DSP power ON sequence — This sequence is used to power on the DSP core.

    1. Unmask the wakeup event: by default, all DSP interrupts are masked as wakeup events. To unmask a

    wakeup event, write the corresponding bit in registers DSS_REG.PWRSMWAKEMASK[0-2]. The 96-bit

    configuration corresponds to the [95:0] interrupt lines to the DSP.

    2. If the program code must be downloaded into the DSP L2 memory before starting the DSP execution,

    then set the DSS_REG.GEMPWRSMCFG4.PWRSMLRSTHALT bit to 0x1.

    3. Trigger the wakeup: when an unmasked interrupt is generated to the DSP, a wakeup trigger is

    generated.

    4. Wait for GEM to be powered on by polling the field DSS_REG.GEMPWRSMCFG4.PWRSMSTATE for

    the value 0xB. SW can now configure and trigger the DMA for the program code download.

    5. When the program code is completed, SW can now release the halt by clearing the

    DSS_REG.GEMPWRSMCFG4.PWRSMLRSTHALT bit; DSP begins execution.

    6. Follow the steps in the DSP Execution on Power ON section below.

     

    He only seems to be configuring DSS_REG.GEMPWRSMCFG4.PWRSMLRSTHAL and DSS_REG.GEMPWRSMCFG4.GEMEVENTMASK.

    I do not see any Wake up trigger in his sequence. Please check.

    Could you verify if you have the exact flow given in TRM section mentioned above?

    Regards,

    Jitendra

  • Hello Jitendra,

    thank's for the info but unfortunately we are going a bit in a circle. My previous questions was exactly related to the following statement in the manual:

    3. Trigger the wakeup: when an unmasked interrupt is generated to the DSP, a wakeup trigger is

    generated.

    I am aware of the fact that a wakeup event is required and that it needs to be unmasked. However the TRM makes no mention on how to actually

    trigger (or generate) the wakeup event. On the other side the debug system block diagram (Figure 27-2) shows a "Triggers" module which is not

    shown in the associated table 27-2.

    I was under the impression that those triggers could be used to trigger a wakeup of the DSP. But in any case let me rephrase my question:

    How can an unmasked interrupt - which results in a wakeup event - be triggered from the CR4 debug subsystem?


    Best Regards,

    Wolfgang

  • Hello Wolfgang,

    Just a note based on the latest feedback:

    Reset of DSS (sub-system) is not supported in mmWave Sensor but DSP core reset is possible.

    On top of the above all the sequence, You can use SW interrupts from MSS that go to the DSP interrupt map. It's used to generate a wakeup trigger from the DSP to finally restart the core.

    Enable the MSS DMM SW interrupt 4 as a DSP wakeup event  :  Reg_Write[0x500006D8] = 0xFFFF7FFF;

    then trigger the MSS DMM SW Interrupt 4 :    Reg_Write[0xFFFFF948] = 0x10;

    Let me know these steps help you further.

    Regards,

    Jitendra

  • Thank's a lot. This does the trick. Please note that even the mentioned registered are in the device XML files they

    are missing from the technical refereence mannual.

    Best Regards,

    Wolfgang