This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TMP61/TMP63/TMP64 – Do I need a capacitor at the voltage divider output of a thermistor?

Expert 6820 points

Replies: 1

Views: 225

Do I need a capacitor at the voltage divider output of a thermistor? 

  • Using a capacitor at the voltage divider is not required and should not be used when using a ratiometric approach.  When not using a ratiometric approach, adding capacitance at the voltage divider output can be used to filter the divider voltage, but it will increase the response time.  However, an alternate solution would be to add a capacitor to Vbias to filter noise in the system. 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.