Part Number: OPT3004
Other Parts Discussed in Thread: OPT3001,
OPT3001 vs OPT3004, what is the difference?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPT3001 and OPT3004 are quite similar devices. OPT3004 is a newer part that adds better angular IR rejection. This is specifically useful in IP camera applications that use infrared LEDs and a dome shaped glass that reflects the IR light from all angles into the light sensor. Both devices are the same size and pin to pin compatible.
Spec changes
Infrared response (850 nm): spec'd over angle in OPT3004
Half-power angle: increased in OPT3004
Measurement drift across temp: increased to 0.02%/degC in OPT3004
Plots added
Figure 3. Spectral Response vs Wavelength from 85° to -85° in 10° Steps Normalized to each Angle of Incidence