Other Parts Discussed in Thread: MMWAVEICBOOST
Hi,
We need to be able to use the rl_sensor API to generate a CW for production and certification testing - there is no provision to use DCA1000 and mmWave studio for this test.
If I look into the SDK3.3 I see the API rlDeviceSetContStreamingModeConfig() should be the one to use but it also says in the comments the below -
This API is valid only when mmWaveLink instance is running on External Host Processor
Does this mean that i cannot us on IWR6843 ? If not then how should I proceed ?
Thanks.