Other Parts Discussed in Thread: DRV5055
Can someone recommend whether I can use DRV5055-Q1 for PMSM control?
I need to sense the absolute position and will this give Analog o/p as measure of absolute position?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can someone recommend whether I can use DRV5055-Q1 for PMSM control?
I need to sense the absolute position and will this give Analog o/p as measure of absolute position?
DRV5055 will produce an output relative to the magnetic field the sensor is exposed to
However, the portion of the magnetic field sensed will be relative to magnet and sensor orientations
As the magnet moves or rotates, the sensor will experience a varying magnetic field which will aid in determining the angle of the magnet orientation. However, a single DRV5055 will not be able to resolve absolute position. Aside from minimum, maximum, and zero crossing, there will be two magnet positions for each magnetic field magnitude. To resolve this error, a second sensor placed 90 degrees from the first will help determine the exact angle.
More information regarding the theory can be found in Linear Hall Effect Sensor Angle Measurement Theory.
Additionally, an implementation for detecting angle of a single rotating diametric disc magnet can be found in the DRV5055-ANGLE-EVM.